2020-11-12 04:59 PM
Hi guys,
I have just installed the "STM32cude IDE'' and have a "nucleo F303 RE''.
I'm tryping to create a stm32 project "file -> new -> STM32''. But when initializing everything for the first time, the IDE start dowloading packages and ''stm32cube_fw_f3_v1111.zip'' is one of them. But it always to do so. I have tried many times but no success. I have made researches on the internet, but not much answers either. Some people say to download it manually but I can't find this package.
As you can see on the image, the workspace as been created in ''Guest/STM32CubeIDE/workspace/'' which I think is good.
What do you think is the problem? And what can I do to start creating my 1st project.
thanks in advance.
Solved! Go to Solution.
2020-11-12 08:36 PM
It's generally bad form to post a duplicate question, especially after only 8 hours.
Could be an issue with your firewall/proxy blocking access. Could be STs site is down. You could try downloaded standalone STM32CubeMX and trying it there.
2020-11-12 08:36 PM
It's generally bad form to post a duplicate question, especially after only 8 hours.
Could be an issue with your firewall/proxy blocking access. Could be STs site is down. You could try downloaded standalone STM32CubeMX and trying it there.
2020-11-13 01:28 AM
Hello @FMike.1 ,
Welcome to the STM32 Community 😊.
I have successfully download and install this package from ST web and STM32CubeMX !
Maybe it was just a browser-cache issue, or slow server response. So, I suggest to clean your cache and try again.
However, to find a way out of that situation, I send you the needed package via drive: STM32CubeF3 V1.11.1
Please select the post as a "Best Answer" if it solved your problem.
Imen
2020-11-15 09:50 AM
Hi TDK, Hi Himen,
Thank you for your answers guys. i had a bad manipulation with the 1st post but couldn't find how to delete. But I take note. thanks.
I'll try your suggestions and come back to you to let you know how it went.
Thanks in advance guys.
2020-11-18 02:17 PM
Hi Guys,
thanks for your help both of you.
The problem was the firewall proxy.
I couldn't download your file Imen just to tell you how it was.
But it's fixed now.
Thanks