cancel
Showing results for 
Search instead for 
Did you mean: 

P-NUCLEO-IHM03 Motor Profiler for Gimbal Motor GBM2804H-100T

Tore Kallevik
Associate II

Motor Profiler and P-NUCLEO-IHM03 does not work (time out every time).

GBM2804H-100T Motor Specifications:

Configuration: 12N14P

Max Rotation Speed: 2180

Test Current: 0.0099A

Max Current: 5A

Which settings for Motor Profiler works with the P-NUCLEO-IHM03 ?

5 REPLIES 5
Laurent Ca...
Lead II

Dear @Tore Kallevik​ 

Could you attach a screenshot of your Motor Profiler settings into this thread?

Thanks by advance.

Best regards

Laurent Ca...

Tore Kallevik
Associate II

0693W000005A8JbQAK.png0693W000005A8HjQAK.png

Tore Kallevik
Associate II

Often when I Start Profile the Rs and Ls values of Electrical Model becomes wrong:

0693W000005A8KdQAK.png

Laurent Ca...
Lead II

​Dear @Tore Kallevik​ 

One of our team members reproduced your configuration and setup and met the same error.

For some motors, most especially small ones, you have to try to tune a little bit more.

In your case, if you replace Max current of 0.5 Apk by 0.1 Apk (in your first screenshot), the Motor Profiler runs and converges.

Could you try this and keep us informed on the outcome?

Best regards

Laurent Ca...

Tore Kallevik
Associate II

Hi Laurent,

First, thanks for getting back to me on this.

However 0.1 Apk did not work with my Nucleo G431 Revision Y:

0693W000005CxG7QAK.jpg 

But replacing the Nucleo-G431 with Nucleo-F303RE fixes everything:

Now my motor profiler finally works.

Rgds, Tore