cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303AH vs ISM303DAC differences.

TBart.1
Associate II

Hi. What are the differences between them?

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Bacteriusartnik​ ,

ok I just see you have edited the post.

LSM303AH and ISM303DAC are very similar chip: the main difference is that the ISM303DAC ha been qualified in industrial conditions, while the LSM303AH ins standard conditions.

If your application is not industrial, you can use the LSM303AH.

-Eleon

View solution in original post

4 REPLIES 4
Eleon BORLINI
ST Employee

Hi @Bacteriusartnik​ ,

are you referring to the LSM303DLH, right?

The ISM303DAC device has in general better performances than LSM303DLH one, especially regarding:

  • higher resolution for the accelerometer (sensitivity on 16 bits);
  • wider magnetometer full scale;
  • industrial grade qualification;
  • currently available on the market.

-Eleon

TBart.1
Associate II

Hi @Bacteriusartnik​ ,

ok I just see you have edited the post.

LSM303AH and ISM303DAC are very similar chip: the main difference is that the ISM303DAC ha been qualified in industrial conditions, while the LSM303AH ins standard conditions.

If your application is not industrial, you can use the LSM303AH.

-Eleon

AJame.3
Associate

Hi,

I have a related question: Can we use ISM303 for Tilt-compensated compasses application as well? When checking the datasheet, Tilt-compensated compasses is mentioned only in the 'Applications' of LSM303 and not in ISM303.

I was looking to ISM303 for a Tilt-compensated compass application. Can you please share your comments?

Thanks

Akshay