cancel
Showing results for 
Search instead for 
Did you mean: 

SPC574K-DSP(V2.00) board with UDE STK 50 debugger unable to connect after laptop shutdown

CoolMo
Associate III

Hallo everyone.

I am evaluating this platform and I got it to work with the UDE STK debugger env.

unfortunatley when I shutdown my laptop at the end of the day, it seems to loose all the driver settings.

The morning after when I try to connect to the boar dit gives me this error message:

Message from component 'PpcJtagTargIntf' :

Can't connect target !

Message from component 'PpcJtagTargIntf' :

No JTAG client found !

Please check:

- target power supply

- JTAG cable connection

- target configuration

I am on W10 Pro x64.

I connect the eval board USB cable to the dock (but it has same behavior even if I use the laptop's own ports)

The drivers for FTDI and PLS USB JTAG adapter are installed and configured in device manager settings:

0693W000004JEalQAG.png

I don't like having to reinstall the UDE STK 5.0 every day...

Has anyone faced the same problem? how did you fix it (if ever)?

Thanks in advance

Maurizio

1 ACCEPTED SOLUTION

Accepted Solutions
CoolMo
Associate III

Greetings Every1,

I answer to myself: by disabling in WIndows Device Manager one of the two interfaces, the debugger now works OK.

Right-click, select disable.... (you can re-eanble at anytime)0693W000004JQ4wQAG.png 

View solution in original post

1 REPLY 1
CoolMo
Associate III

Greetings Every1,

I answer to myself: by disabling in WIndows Device Manager one of the two interfaces, the debugger now works OK.

Right-click, select disable.... (you can re-eanble at anytime)0693W000004JQ4wQAG.png