cancel
Showing results for 
Search instead for 
Did you mean: 

[BUG] CubeIDE example selector misses many actually supported boards

MEvst.1
Associate

Hi,

I just installed IDE v1.4.0. I can't find any example for the Nucleo-L476RG board from the Example Selector tabof the Target Selection window. The provided list of the boards doesn't contain L4 family as well as many other families (Lx, F1 and etc.).

The examples can be found directly from the MCU family packs in the same way as for the boards included into the selection list. So the examples do exist while IDE doesn't find them.

So I think that it is just a bug in the IDE configuration files.

BR,

Mikhail

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

See:

https://community.st.com/s/question/0D53W00000EHEzW/how-to-install-f0-examples-to-cubeide

> Example Selector:

>  The feature is functional only for the examples related to the STM32F4, STM32F7, STM32G0, STM32G4, STM32H7, STM32L5 and STM32WB Series

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

See:

https://community.st.com/s/question/0D53W00000EHEzW/how-to-install-f0-examples-to-cubeide

> Example Selector:

>  The feature is functional only for the examples related to the STM32F4, STM32F7, STM32G0, STM32G4, STM32H7, STM32L5 and STM32WB Series

If you feel a post has answered your question, please click "Accept as Solution".
MEvst.1
Associate

Thanks TDK,

It is clear now.

So it is not a bug. It is known limitation.

Would be good to have limitations like this more visible when trying to use the feature.

BR,

Mikhail