cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I'm using STM32H743IIT6 with LTDC configurations and when I'm using internal clock, LTDC works fine but when I use external crystal nothing works . What can be the problem?

NBehe.1
Associate

And when I'm going to find the problems using DEBUG mode it gives me this error:

Cannot access Memory

*** error 122: AGDI: memory read failed (0xFFFFFFFE)

Cannot access Memory

And this are is LTDC configuration and Clock configuration:0693W000004IaWAQA0.png0693W000004IaWKQA0.png

0693W000004IaWPQA0.png

0693W000004IaWUQA0.png

1 REPLY 1
MM..1
Chief II

?? Frame buffer start address 0 ?? and why two layers

for your size and dot clock frame rate is 90Hz , isnt to big? Try change 12Mhz to 8MHz...