cancel
Showing results for 
Search instead for 
Did you mean: 

migration from MX25L512G to MT25QL256ABA8ESF

GMoha.1
Associate II

I used disco board stm32f769i in external flash application and it works well then I used the same microcontroller type with another external flash module  MT25QL256 and the written data is corrupted .

I think it is configuration problem so what the principle configuration should I review?

and is there any flashing algorithm code for MT25QL256 IC ?

2 REPLIES 2

There might be some BSP code for the Micron/ST parts.

I think the 512Mbit​ is more popular.

You might be able to use or repurpose some of the other loaders, but you'd need to be using the same pin configurations.

Writing loaders is a bit of a task​.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..

I used the same pin configuration but when reading data it seems like this some data burnt and other not

is there any clock or mode configuration need to be updated

0693W000004IZu6QAG.png