cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746GDISCO, STM32CubeIDE, Warnrings

AD�?b
Senior

I have such a warning. Why?

Invalid project path: Include path not found (C:\Users\48502\STM32CubeIDE\workspace_1.4.0\start\FATFS\App).   start      pathentry   Path Entry Problem

Andrzej

5 REPLIES 5
TDK
Guru

Does that path exist?

If you feel a post has answered your question, please click "Accept as Solution".

I don't use FATFS. I don't have it turned on.

mattias norlander
ST Employee

Look in your include paths for the project, is this path listed? If it is not relevant, just remove it from include paths to get rid of the warning..

mattias norlander
ST Employee

There are some bugs related to removal of include paths in CubeMX/CubeIDE. I am guessing that you once had FatFS enabled, and then disabled the module. When enabled MX added this include paths for you. Then later when disabled it was not properly removed... If assumption correct, then this is a known issue and ticket exists.

My previous reply should be sufficient to solve this problem, but it can happen again when enabling/disabling middleware components in MX.

OK