2020-09-24 07:08 AM
Hello
I have the problem with USART baud rate in STM32F09x. I want to use baud rate: 9600, 19200, 38400, 57600, 115200bps with data length - 8 bits, parity and one stop bit.
I can connect to the device at all speeds except 19200.
Microcontroller uses HSI 48 MHz clock.
Where is the problem ?
Thank you for help.
2020-09-24 07:46 AM
2020-09-24 08:41 AM
> I can connect to the device at all speeds except 19200.
How exactly does "can not connect" exhibit itself?
Note, that HSI is +-1% only at 25 deg.C and VDDA = 3.3 V. Also, some Cube incarnations on some families tend to spoil the internal RC oscillators trim, so check RCC_CR.HSITRIM.
JW
2020-09-24 10:12 PM
Hello,
I am testing transmission and I have noise error for 19200 speed in receive mode. I used 2 diffrent master and I have this error in my microcontroller. It works as a slave.
Pferd