2020-09-22 12:42 PM
Hi at all,
I bought a NUCLEO-F401RE and a X-NUCLEO-IHM03A1.
I've created a STM32CubeIDE project starting from the example "IHM03A1_ExampleFor1Motor" included inside the "STM32CubeExpansion_SPN3_V1.6.0" package.
I downloaded the project on Nucleo F401RE board and everything works fine.
Now I'm trying to integrate this motor example on my project that manage:
- TIM2 32 bit counter (external encoder 1)
- TIM5 32 bit counter (external encoder 2)
- 2 external interrrupt (encoders index to reset the counter values)
- USB OTG used to communicate with a computer as virtual com port
But when I download this new project the firmware hang when I call
BSP_MotorControl_Init(BSP_MOTOR_CONTROL_BOARD_ID_POWERSTEP01, NULL);
Obviusly my project without the motor section works fine.
I think there are some mismatch between the the sample motor project and my project configurations.
Eg:
this is the clock config of the motor sample project
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Enable Power Control clock */
__PWR_CLK_ENABLE();
/* The voltage scaling allows optimizing the power consumption when the device is
clocked below the maximum system frequency, to update the voltage scaling value
regarding system frequency refer to product datasheet. */
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/* Enable HSE Oscillator and activate PLL with HSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
MyErrorHandler(0);
}
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
MyErrorHandler(1);
}
}
This is my clock config auto generated by STM32CubeIDE
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 72;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 3;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
I've also welded a XTAL 8 Mz + 2 capacitors on my NUCLEO F401RE and cut off the ST-Link debugger.
Any suggestions will be greatly appreciated.
Thank you so much.
2020-09-23 09:14 AM
Dear @addebito
What is the MC-SDK version number you use?
Best regards
Laurent Ca...
2020-09-23 12:02 PM
Dear Laurent,
thank you for your reply.
I've download the "en.x-cube-spn3.zip" at this link:
https://www.st.com/en/embedded-software/x-cube-spn3.html#overview
No MC-SDK but I've created a project by "STM32CubeIDE 1.3.0" starting from the single motor example application contained inside the zip file
.\STM32CubeExpansion_SPN3_V1.6.0\Projects\Multi\Examples\MotionControl\IHM03A1_ExampleFor1Motor
Best regards.
2020-09-28 07:27 AM
@Laurent Ca... do you have any suggestions?
If there's someone else that has an idea to understand how to check / verify the problem... please let me know.
Thank you.
Best regards.
2020-09-29 12:43 AM
Dear @addebito
Could you give us more details about the motor(s) you use?
Best regards
Laurent C...
2020-09-29 02:23 PM
Dear @Laurent Ca... ,
follow the motor specification but IMHO I don't think it could be a motor problem because when I download and run the example "IHM03A1_ExampleFor1Motor" included inside the "STM32CubeExpansion_SPN3_V1.6.0" package, everything works fine.
I see the motor movements as described through the comments inside the source code.
The problem appear when I merge the 2 projects.
Anyway, this is the motor specifications
Step Angle: 1.8°
Step Angle Accuracy: ±5% (full step, no load)
Resistance Accuracy: ±10%
Inductance Accuracy: ±20%
Temperature Rise: 80 °C Max.(rated current, 2 phase on)
Ambient Temperature: �?20 °C ~ +50 °C
Insulation Resistance: 100 MΩ Min., 500VDC
Dielectric Strength: 500 VAC for one minute
Shaft Radial Play: 0.02 Max. (450 g�?load)
Shaft Axial Play: 0.08 Max. (450 g�?load)
Current (A/Ø): 4.2
Resistance (Ω/Ø): 0.8
Inductance (mH/Ø): 3.0
HoldingTorque (N.cm): 300
DetentTorque (N.cm): 12.0
RotorInertia (g.cm2): 780
Bi/Unipolar (# of Leads): Bi (4)
Weight (g): 1600
Length (mm): 90
2020-10-15 07:33 AM
Dear @addebito
I am in the team working on the MC SDK and have no idea to the content of "STM32CubeExpansion_SPN3_V1.6.0" package.
Sorry to not be able to help you more.
Is there someone in the STM32 Community able to help @addebito on this problem?
Thanks by advance.
Best regards
Laurent Ca...
2020-10-15 07:50 AM
The motor users in my experience are not heavy forum participants.
If there are issues with the clocks you need to make sure they are starting properly, and not going into Error_Handler()
Zeroing the local/auto variables is strongly suggested as they will otherwise contain random junk.
Cutting of the ST-LINK is going to make debugging more difficult. You really need to inspect the state of the MCU and peripherals to see exact where it has stopped, if it has actually crashed or faulted, or is simply waiting for a response from a peripheral that's not being clocked, etc.
At a minimum I would recommend instrumenting Error_Handler() and HardFault_Handler() with output of actionable data to a serial port.
2020-10-15 08:02 AM
I think, this is just a problem of conflicting Pins.... I don´t know much about the used Nucleo-Board (esp. the pinout...), but that´s, where i would begin to search. There are just a few possibilities: first wrong SPI-settings (SPI is used to communicate with the expansion board) and second: forget about the step-signal pin (not used in examples) and maybe also about "busy" and/or "flag". For these two pins: just delete the according initialization code and especially the Interrupts ! The Flag Interrupt is fired at startup and there´s a high chance of being the cause for the crash. Give it a try and if your project works... you´re on the right way 😉
/Charly
P.S.: check the pinout settings in the ihm03a1 example: You need SPI-pins, correct SPI-setup (parameters) and maybe (if still available in your hardware) flag and busy - pins correctly configured. Leave the rest (clock settings and so on) untouched in your project. Then merge just the libraries, example code from mainloop and errorhandler (also in main.c of example), as well, as according interrupt handlers from stm32f4xx_it.c
2020-10-15 08:34 AM
just tried... That powerstep01-package: Be glad, you have never seen it xD For users with less experience, the code inside is horrible to read and to understand...