cancel
Showing results for 
Search instead for 
Did you mean: 

Dear Ladies and Gentleman I'm a student of the University HSLU. At the moment I have been working on an porject in which I have to implement a controllsystem that is controlling and measuring the temperature and values in a bio reactor.

HMate.1
Associate

The bio reactor has bone marrow inside of it and this is being analysed for the properties of microgravitation.

I would use a NUCLEO-F303K8 microcontroller. The system must endure a maximum accelaration of 10G due to the fact that it will be used later on in a Fighter-Jet. My question being now, can the MCU work and function properly under such circumstances?

1 REPLY 1
TDK
Guru

The MCU will have no problem running in a 10g environment.

If you feel a post has answered your question, please click "Accept as Solution".