cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE, How to use Real Time variables??

Bryan_KIM
Associate II

Hello, ​

I am using the STM32 Cube IDE.

I want to monitor real-time variables through debugging mode.

But it doesn't...

How use to Real-Time variables??​

0693W000003RVLGQA4.png

0693W000003RVLQQA4.png

10 REPLIES 10
TDK
Guru

Add them on the live expressions tab. It's buggy on restarts, you usually have to re-enter them when you re-run, but it works.

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for the answer.

I didn't understand the meaning of this.

Excuse me. How should I set it up?

Bryan_KIM
Associate II

Do you mean this?0693W000003RVN7QAO.png

TDK
Guru

The "Live Expressions" tab is two tabs to the right of the "Expressions" tab on your last screenshot.

If you feel a post has answered your question, please click "Accept as Solution".

I think it's mean.

Is it right??

But It isn't real time variables...

It has a fixed value.

I toggled it every second by program.

0693W000003RVOUQA4.png

TDK
Guru

Works for me. Make sure your variable exists and the compiler isn't optimizing it out.

If you feel a post has answered your question, please click "Accept as Solution".
Bryan_KIM
Associate II

I used ST-LINK/V2.

Target mcu is STM32G030C8T.​

VDD

GND

SWCLK

SWDIO

Debug Setting.

0693W000003RVUNQA4.png

I programmed the variable to increase by 1 every second.

However, after changing from the initial value 0 to 1, nothing has changed.

I used ST-LINK/V2.

Target mcu is STM32G030C8T.​

VDD

GND

SWCLK

SWDIO

Debug Setting.

0693W000003RVUNQA4.png

I programmed the variable to increase by 1 every second.

However, after changing from the initial value 0 to 1, nothing has changed.

Could I send it to you?