cancel
Showing results for 
Search instead for 
Did you mean: 

Is it needed for host pc to use static ip when working with LwIP ethernet?

Lpadd.1
Associate

Is it needed for host pc to use static ip when working with LwIP ethernet?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

LwIP can use DHCP, provided you have a DHCP server somewhere.

Static IP can be easier to set up.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
TDK
Guru

LwIP can use DHCP, provided you have a DHCP server somewhere.

Static IP can be easier to set up.

If you feel a post has answered your question, please click "Accept as Solution".
Lpadd.1
Associate

@TDK​ If I use a static ip on my host pc and a static ip on the stm32, do they have to be set differently or do they need to be the same?

TDK
Guru

They should be different. Two devices on a network should never have the same IP.

If you feel a post has answered your question, please click "Accept as Solution".