cancel
Showing results for 
Search instead for 
Did you mean: 

Is it Compatible Marvell 88E1116R PHY chip for STM32F407 ?

KD.3
Associate

I am using STM32F407 Controller For Ethernet Application , then Marvell 88E1116R PHY Chip i want to use with STM32F407 , so is it Compatible ?

3 REPLIES 3
TDK
Guru

STM32 doesn't support gigabit ethernet.

If you feel a post has answered your question, please click "Accept as Solution".
KD.3
Associate

Thank you for your Answer, can i use 100MBPs or 10 MPBs with this Marvell 88E111R Phy Chip, My doubt is STM32F407 supporting MII/RMII and Marvell 88E1116R PHY Chip supporting GMII/GRMII so can i Interface??

if not possible which Phy IC i should use ??

thank you..

TDK
Guru

> Thank you for your Answer, can i use 100MBPs or 10 MPBs with this Marvell 88E111R Phy Chip, My doubt is STM32F407 supporting MII/RMII and Marvell 88E1116R PHY Chip supporting GMII/GRMII so can i Interface??

I don't know enough to know if GMII is backwards compatible with MII. Maybe it's like USB3 and you just have to wire it correctly. Not sure.

> if not possible which Phy IC i should use ??

Any PHY that supports MII or RMII should work. You could use one used on an ST board if you wanted.

If you feel a post has answered your question, please click "Accept as Solution".