cancel
Showing results for 
Search instead for 
Did you mean: 

we have chosen vl53l0x for our product. Before that we bought x nuculeo expansion board and tested(without cover glass),everything is working fine.But after placing cover glass , the sensor first gave measurement as 0mm always.

ANANTH
Associate

Then we tried to do calibration steps as per datasheet, but the offset we are getting is -25000(we placed the white object at 100mm) and cross talk is 0.

SOC : nrf52840

RTOS : Zephyr

GITHUB link for driver : https://github.com/zephyrproject-rtos/hal_st

My doubt is on driver where it is doing calibration for offset and cross talk

Line number 141 in this file, https://github.com/zephyrproject-rtos/hal_st/blob/master/sensor/vl53l0x/api/core/src/vl53l0x_api_calibration.c ,xTalkCalDistanceAsInt will become 0 because

it is shifted by 16 places.If this is the problem then so many places it is happening.

Can anyone help me solve this problem.Thanks in advance.

2 REPLIES 2
John E KVAM
ST Employee

The hardware works in 10.2 format. that is if an offset is 25mm the hardware would give 25<<2. So two binary bits to the right of the implied binary point. (Almost like a decimal point, but in base 2).

However in the ST code someone thought that was odd, and though it would be easier for people to think in thousandths. So the multiplied the 25<<2 by 250 to give thousandths of millimeters - or micrometers.

The code is self-consistent. That means if you do the calibration and get a number, and then put that number back through the same set of software, it will work - even though the number looks odd.

To get a number that makes sense simply divide that number by 1000 and you get the offset in millimeters.

a -25mm is a very typical offset, even though it got left shifted by 2 and then multiplied by 250.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.
ANANTH
Associate

what about this line for cross talk https://github.com/zephyrproject-rtos/hal_st/blob/5b3ec3e182d4310e8943cc34c6c70ae57d9711da/sensor/vl53l0x/api/core/src/vl53l0x_api_calibration.c#L141 where xTalkCalDistanceAsInt becomes 0(because of shifting) and following condition(xTalkStoredMeanRange >= XTalkCalDistance) becomes true always, so i am getting 0 always.Is this also correct?