cancel
Showing results for 
Search instead for 
Did you mean: 

STPMIC1 efficiency at low load

PGE
Associate III

Dear all,

I am looking to use the STPMIC1 in one new STM32MP15x design which will spend most of this time in standby mode.

I am looking for STPMIC1 buck efficiency at light load (~1mA). In the datasheet there is numbers only for 150mA, 750mA and 1A. Is there any additonal numbers or graphics available somewhere ? I can see there is a special LP mode for light load but there is no indication about efficiency in LP mode.

Many thanks in advance for your help

1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @PGE​ 

Did you notice Figure 3 to Figure 6 in DS ?

They contains efficiency for bucks in all range from 0.0001A to 1A in both HP and LP mode.

Isn't it what you are looking for ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @PGE​ 

Did you notice Figure 3 to Figure 6 in DS ?

They contains efficiency for bucks in all range from 0.0001A to 1A in both HP and LP mode.

Isn't it what you are looking for ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PGE
Associate III

Yes thanks ! I don't know why I didn't notice them...