cancel
Showing results for 
Search instead for 
Did you mean: 

Dear fellow geeks, We'r using a Nucleo-f103RB to program a STM32L010k4T6. We ar able to write a PIN high and write a pin LOW we can also use the SPI. The only problem we have is with uart. We can't seem te get it to work.

Rgoss.1
Associate II

In the datasheet https://nl.mouser.com/datasheet/2/389/dm00440565-1799229.pdf0693W000003CCXcQAO.jpg

is stated that the uart and the SPI are part of two different alternate functions. The error message and the code will also uploaded if needed.

1 REPLY 1
Uwe Bonnes
Principal II

What kind of programming are you trying to achieve? Your question is totally unclear.