cancel
Showing results for 
Search instead for 
Did you mean: 

Incorrect Total Width size at LTDC / CubeMX 6.0.0 / FW_H7_V1.8.0

Panchev68
Senior

This is from CubeMX 6.0.0 / FW_H7_V1.8.0

Total Width is same as Horizontal Front Porch

0693W000003ByPZQA0.png

and this is for CubeMX 6.0.0 / FW_F4_V1.25.0 with the same parameters

(everything looks good here)

0693W000003ByPPQA0.png

1 REPLY 1
Amel NASRI
ST Employee

Hi @Panchev68​ ,

Could you please precise the selected device? You can also share your .ioc so it will be easier to reproduce issue.

I tried with STM32H743VGTx as device and settings are different for LTDC.

-Amel

PS: Please submit your question under STM32 MCUs Q&A space and add relevant tags, otherwise it will have less chance to be reviewed if you submit it under Bug-Report.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.