cancel
Showing results for 
Search instead for 
Did you mean: 

STemWIN windows with LISTBOX increase memory used and do not release the memory

Ckerl.1
Associate

I have inherited a GUI project that has a memory leak which I tracked down to the use of the LISTBOX.

If I remove the LISTBOX the memory usage never rises however if I utilize a LISTBOX even if empty memory used by STemWIN will rise until it runs out and crashes.

Is this a known issue,or do I have an implementation error. Any examples of correct implementation or help would be appreciated.

0 REPLIES 0