cancel
Showing results for 
Search instead for 
Did you mean: 

I have dc motor with encoder hall effect and i want control position i need help for write code. I'm now this platform (have code).

MAvet.1
Associate II

only can't write interrupt command for working

my board with stm32f103

this is a source code

attachInterrupt need to convert for this platform this is written no right

thnak's

i keep file in here

5 REPLIES 5
Laurent Ca...
Lead II

Dear MAvet.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

Yes of course ​

Laurent Ca...
Lead II

Dear @MAvet.1​ 

Could you give more details to the STM32 Community about the material you use (HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)?

And more especially did you use MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @MAvet.1​ 

Any news?

Best regards

Laurent Ca...

Laurent Ca...
Lead II

Dear @MAvet.1​ 

As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...