cancel
Showing results for 
Search instead for 
Did you mean: 

How to download file to device while device had read out protected in use Boot loader command-line?

DChen.3
Associate II
 
2 REPLIES 2
TDK
Guru

I'm pretty sure you can still erase and write memory when RDP is enabled, the process for those would be the same.

Or you could set RDP to 0, program as normal, and set RDP back to 1.

If you feel a post has answered your question, please click "Accept as Solution".

Do it last.. or do it from within

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..