cancel
Showing results for 
Search instead for 
Did you mean: 

evaluation kit of BLDC driver IC L6235

SShin.1
Associate

we want to develope simple BLDC driver in open loop mode with speed and direction control input.I found your IC L6235 which fits to our requirement .

is there any evaluation kit this IC.

1 ACCEPTED SOLUTION

Accepted Solutions
Cristiana SCARAMEL
ST Employee

​Hi @SShin.1​ ​ welcome to ST community.

You can use the EVAL6235Q a 3-phase BLDC motor driver board that allows to test the L6235Q functions (L6235 device in QFN package).

The evaluation board can be driven using the STEVAL-PCC009V2 communication board and the PractiSPIN 2 evaluation software (STSW-SPIN003).

I hope I have been helpful.

View solution in original post

1 REPLY 1
Cristiana SCARAMEL
ST Employee

​Hi @SShin.1​ ​ welcome to ST community.

You can use the EVAL6235Q a 3-phase BLDC motor driver board that allows to test the L6235Q functions (L6235 device in QFN package).

The evaluation board can be driven using the STEVAL-PCC009V2 communication board and the PractiSPIN 2 evaluation software (STSW-SPIN003).

I hope I have been helpful.