cancel
Showing results for 
Search instead for 
Did you mean: 

LoraMac. Only three chanels - how to make more?

SArca
Associate

Hi everyone!

I have stm32L072 chip and sx1272 lorachip.

I had developed a simple end-node device with stm32 lrwan library and endnode example for nucleo board.

Developed by Atollic True Studio.

Versions is: MAC_VERSION= 04.04.02.00 and STM32CubeExpansion_LRWAN_V1.3.1

options that i had used to:

   1)LORAWAN_ADR_ON - true;

   2)Global define REGION_EU868;

   3)server's chanels list:

3.1) FIXED; (servers chanel default);

3.2) FIXED;

3.3) FIXED;

3.4) 867,1 MHz;

3.5) 867,3 MHz;

3.6) 867,5 MHz;

3.7) 867,7 MHz;

3.8) 867,9 MHz;

Questions:

   My firmware program is always send data by three chanels: 868,1MHz, 868,3MHz, 868,3MHz. How can I add the missing channels?

0 REPLIES 0