cancel
Showing results for 
Search instead for 
Did you mean: 

Enable automatic code generation STM32CubeIDE

PGroe.2
Associate III

Hi,

I work with STM32CubeIDE

Version: 1.3.1

Build: 6291_20200406_0752 (UTC)

I somehow managed to disable automatic code generation for altered *.ioc file.

Now it doesn't automatically regenerate the source files according to the changes

I made in the configuration window for my STM32... instead it just shows a bracketed text

besides my *.ioc file in the Project Explorer so I have to click on the "Device Configuration Tool Code Gerneration" button to generate it.

If I remember correctly there was once a question if I want to auto-generate the code.

It seems I denied the question and ticked the "do not ask again" field. How can I revoke that decision?

1 ACCEPTED SOLUTION

Accepted Solutions
Cartu38 OpenDev
Lead II

You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.

By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.​

View solution in original post

1 REPLY 1
Cartu38 OpenDev
Lead II

You can revoke your decision relying on Windows>Preferences>STM32Cube>Device Configuration Tool.

By the way asking for code generation if .ioc editor active if possible either relying on Project>Generate code or pushing gear wheel in the toolbar.​