cancel
Showing results for 
Search instead for 
Did you mean: 

Not able to flash STM32H7B31 Code Menu Launcher

DRAME.1
Associate II

Hi Team

I have tried flashing the Menu launcher code

I see that the device is not doing anything after flashing It gets halted while flashing

I have attached the screen shot

Follwing is the procedure that i followed

Downloaded the code from the

STM32Cube_FW_H7_V1.7.0

In this project i have used use MENU launcher

C:\Users\Deepak\Downloads\en.stm32cubeh7_v1-7-0\STM32Cube_FW_H7_V1.7.0\Projects\STM32H7B3I-DK\Demonstrations\MenuLauncher\STM32CubeIDE

when i try flashing the code i get the follwing error as addtached in the screen shot

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

    InitWhile         : Enabled

Waiting for debugger connection...

Debugger connected

Debugger connection lost.

Shutting down...

I used stcubeprogrammer as well for the programming and i am not able to to flash it

I have selected the

MX25LM51245G_STM32H7B3I_DISCO and then in external programming option i selected the Start programming I see that

18:58:52 : STM32CubeProgrammer API v2.4.0

18:58:55 : ST-LINK SN : 001700373038510234333935

18:58:55 : ST-LINK FW : V3J6M2

18:58:55 : Voltage : 3.29V

18:58:55 : SWD freq : 24000 KHz

18:58:55 : Connect mode: Normal

18:58:55 : Reset mode : Software reset

18:58:55 : Device ID : 0x480

18:58:56 : UPLOADING OPTION BYTES DATA ...

18:58:56 : Bank : 0x00

18:58:56 : Address : 0x5200201c

18:58:56 : Size : 308 Bytes

18:58:56 : UPLOADING ...

18:58:56 : Size : 1024 Bytes

18:58:56 : Address : 0x8000000

18:58:56 : Read progress:

18:58:56 : Data read successfully

18:58:56 : Time elapsed during the read operation is: 00:00:00.002

19:00:32 : Memory Programming ...

19:00:32 : Opening and parsing file: MenuLauncher-STM32H7B3I-DK_V1.0.0.hex

19:00:32 : File : MenuLauncher-STM32H7B3I-DK_V1.0.0.hex

19:00:32 : Size : 1696395 Bytes

19:00:32 : Address : 0x08000000 

19:00:32 : Erasing memory corresponding to segment 0:

19:00:32 : Erasing internal memory sectors [0 10]

19:00:32 : Erasing memory corresponding to segment 1:

19:00:32 : Erasing external memory sectors [0 24]

19:00:37 : Error: failed to erase memory

19:00:37 : Error: failed to erase memory

I am not sure what options to select and how to overcome the GDB SEVER error or the

ERROR IN PROGRAMMING using the STCUBEPROGRAMMER

Note: My switch postion id in FLASH memory on board

0 REPLIES 0