cancel
Showing results for 
Search instead for 
Did you mean: 

Can I load DSP settings into STA369 via i2c

CAsto.1
Associate

We need to tune a set of speakers to the STA369 via DSP. We would like to load the DSP settings onto the chip via i2c preferably via Android drivers in our firmware. Is this possible.

Regards,

Colin Aston-James

1 REPLY 1
Peter BENSCH
ST Employee

These are two questions:

  1. yes, you can change the filter coefficients via I2C, e.g. by using the APWorkBench, please also refer to the UM1545
  2. Android: should be possible if you write the app for it or find someone doing this for you

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.