cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157 FMC NAN,D NCE or NCE2 ?

PMort.1
Associate II

I want to connect a SLC NAND to the FMC controller and boot from it

What CS* must i use (NCE or NCE2) ?

Why i got the "Pin not available for boot step" in CUBEmx when trying to select NCE2 ?

1 REPLY 1
PatrickF
ST Employee

Hello,

only SLC NAND device connected using FMC_NCE is supported as boot source.

You could refer to related wiki page and AN5031.

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.