cancel
Showing results for 
Search instead for 
Did you mean: 

Rest RDP Read Protection

As.51
Associate III

Hi, I have the STM32F427VI, I don't know how this happend but now is read/write protected Level1. How can I reset this, I want to disable read protection at all to burn my application.

Now I can't read the memory 0693W000001qVU5QAM.pngwith STM Utility with J-TAG and coudn't erase memory with Demonstrator GUI via RS232. Please see the attached image.

6 REPLIES 6
TDK
Guru

Uncheck all sectors on the bottom and change Read Out Protection in the top-left to Level 0 and apply.

If you feel a post has answered your question, please click "Accept as Solution".
As.51
Associate III

I tried this but I get the error: Could not set Option bytes!

Please see the attached picture. Thank you for your help:)0693W000001qWgbQAE.png

Piranha
Chief II

Set "Connect Under Reset" and do full chip erase.

This is not working. Please see the images attached

0693W000001qjM5QAI.png

0693W000001qjLvQAI.png

As.51
Associate III

I managed with the option bytes to remove the read only but when I conenct with JTAG I still get the message that the MCU is ready only0693W000001qjSwQAI.png

As.51
Associate III

I managed to do it by removing all jumpers in the board.Thanks!