2020-06-09 10:07 AM
Hi 🙂
I found something quite strange, it seems that:
1) On DAC Channel 1 - the output buffer does not work (a 10kOhm load brings the voltage down), but it's output is inverted (as expected)
2) On DAC Channel 2 - the output buffer does work (maintains voltage with a 10kOhm load), but it's output is not inverted
My test setup:
The results:
With Output buffer OFF on both channels, the sine wave is not inverted, and the voltage is sinked to max 1.5V - this is as expected.
With the output buffer ON on both channels, you can see that Channel 1 (yellow) is inverted but its output is still sinked, and that Channel 2 (blue) is not inverted but its output is maintained with the load.
Note 1: I desoldered the SB21 to disconnect the LED 2 from the output of the Channel 2 - but even before I did the results were almost the same (it just added a load and a small cut at the top of the waveform).
Note 2: I also double checked the value of the DAC->CR register with the debugger, it shows:
I went through the datasheet but it does not say anything about differences between the DAC's. I guess I am doing something wrong somewhere?
Thank you!! :D
2020-06-09 02:02 PM
Why would inverting be normal? It's not.
Reminds me of https://community.st.com/s/question/0D50X00009XkZsS/my-dac-outputs-inverted-values-0000-33v-and-4095-0v
JW
2020-06-09 11:42 PM
Thanks Jan for your reply - you are on every post ha ha! :D
Very interesting that post - that's exactly my issue, so I guess I just destroyed the buffer then...
And yes I would expect the buffer to invert the output, since it is configured as an inverting opamp with G=-1 ?
See from https://www.st.com/resource/en/application_note/dm00129215-extending-the-dac-performance-of-stm32-microcontrollers-stmicroelectronics.pdf @page 5:
2020-06-10 01:35 AM
> Very interesting that post - that's exactly my issue, so I guess I just destroyed the buffer then...
I don't know, I just posted a link. Maybe you should try on a different piece of hardware the same software.
> And yes I would expect the buffer to invert the output, since it is configured as an inverting opamp with G=-1 ?
Interesting. Why wouldn't the RM mention that?
I don't remember whether I ever used the DAC with buffer.
JW
2020-06-11 09:25 AM
Well it does match exactly the results I am getting. Thanks anyways.
And I guess by "RM" you mean the datasheet? If so that is true I double-checked and it is not written anywhere, only on that other ST document...
2020-06-11 01:12 PM
STM32 uses a set of reference materials, some more general for the family, other specific to the particular model:
PM = Programing Manual, here PM0214 (describes the ARM processor/core)
RM = Reference Manual, here RM0390 (describes a family's buildup and peripherals from programming/functional point of view)
DS = Datasheet, here DS10693 (describes particular model, giving overview and model-specific set of parameters)
ES = Errata Sheet, here ES0298 (model-specific errata)
Then there is supplementary material: AN (application notes), TN (technical notes), UM (user manual, usually for software) and maybe some other which are mostly promotional/marketing.
JW
2020-06-12 03:50 AM
Nice to know! Thank you Jan!
2020-06-18 02:02 PM
Just FYI - I tested it on my Disco-L1 board and it works as expected: no inversion and the DAC can handle a light load, same on both channels.
2020-06-18 03:17 PM
Thanks for coming back with this info.
JW