cancel
Showing results for 
Search instead for 
Did you mean: 

have a problem in stm32CubeMx

zxin.2116
Associate II

I have use stm32CubeMx for code generate.

In a new version I cannot find the generate code button.

old version has the generate code button .0693W000001qB7aQAE.png

but the new one is none

0693W000001qB7kQAE.png

5 REPLIES 5
Khouloud ZEMMELI
ST Employee

​Hello @Community member​ 

Which CubeMX version are you using ?

And could you please uninstall this one then download the 5.6.1 version from site ? "https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html "

Thanks

Khouloud

ver5.6.1 can not use the stm32WL, I used the STM32CubeMX 6.99.1-D37 version ,

http://www.stmcu.org.cn/module/forum/forum.php?mod=viewthread&tid=624888&highlight=wl

I intsall unintsall several times, and read the note again again:

//*********************************************************************************************

Installing and running STM32CubeMX 6.99.1-D37

Supported operating systems and architectures

  • WindowsÆ 10: 32-bit (x86), 64-bit (x64)

Software requirementsThe Java Run Time Environment 1.8_45 64-bit must be installed.

Limited validation is done with Javaô 11.

Javaô 7, Javaô 9 and Javaô 10 are not supported.

After Oracle announcement related to ëEnd of Public Updates for Oracle JDK 8í, you can access to OpenJDK via https://adoptopenjdk.net/.Installing STM32CubeMX standalone versionTo install STM32CubeMX, follow the steps below:

  • Download STM32CubeMX installation package from www.st.com/stm32cubemx.
  • Extract (unzip) the whole content of the the latest STM32CubeMX installation package from http://www.st.com/stm32cubemx into the same directory
  • Check your access rights and launch the installation wizard:
  • on Windows
    • Make sure you have administrators rights
      • Double click on the SetupSTM32CubeMX-6.99.1-D37.exe file to launch the installation wizard

//*********************************************************************************************************

Khouloud ZEMMELI
ST Employee

​As disccued with @Community member​ , the official CubeMX version will be available to download w28 from site  (which supports the WL)

Best Regards,

Khouloud

Khouloud ZEMMELI
ST Employee

​@Community member​  WL will not be supported in 6.0.0, it will be for 6.1.0.

Best Regards,

Khouloud