cancel
Showing results for 
Search instead for 
Did you mean: 

What families have oversampling on the ADC(s)?

Fanuc30
Associate II

I thought I ran into a bug when CubeMX could not configure oversampling for an F767 after I had used it on the less powerful L4. Read the reference manual and understand it is not there.

Could not find which non-L families DO have oversampling. Hence the question.

2 REPLIES 2

ST unfortunately does not have a list of variants of the peripherals' IPs used in various STM32 families.

The ADC in the 'Fxx tend to be substantially different from the ADC in the 'Lxx, so I'd said you can expect oversampling to be in 'L0/'L4/'L5 (not in the older 'L1 though). It's probably also in 'H7 and the 'G0/'G4. You'll need to check yourself.

JW

Thanks Jan. I even tried to find the logic myself by going over products, but I have to open reference manual actually.