2020-05-26 05:16 AM
If I modify something in the .ioc file, afterwards it always shows a dialog that Code generation is required. Please add a checkbox that never show this dialog again because this is very annoying.
Lot of people not rely 100% on the .ioc file, like me.
Thanks.
2020-05-26 10:55 PM
Or you can just hack your .ioc file removing 'isbadioc=true' line ...
But to be honnest not understand why such dilaog is a pain to you ? Such dialog only happens if you've done some device configuration without moving up to source code update.
+ If not trusting device configuration tool work means you're not using it so no issue because .ioc file content remains unchanged so ... no dialog.
+ If using device configuration tool what about interest to only play with its UI without getting by the end result of such activity i.e. .c/.h files update ...
Maybe sharing your way of working would help here ...
2020-12-08 11:27 PM
I have a similar problem. The code generator has run without problems, but the compiler still opens this dialog and warns me about "requires code generation".
I have to admit, that I once closed the ioc file without code generation and dismissed the dialog warning me about that. I went back to IOC and did a code generation "Ctrl-S" or "CTRL-K", the code was generated, but the dialog sill remains.
(CubeIDE 1.5.0, STM32F207)
Side note: In my ioc file, the bad-ioc-flag is false
isbadioc=false
Johannes