cancel
Showing results for 
Search instead for 
Did you mean: 

Error debugging with two ST link at the same time

ICohe.1
Associate III

Trying to debug with two st link V2 at the same time, I started the first and then tried to start the second. Firstly I had to select the correct serial number for the second ST link but then I got the error: 

Failed to bind to port 61234, error code -1: No error

Failure starting GDB server: TCP port 61234 not available.

Here is the output:

 
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
 
Starting server with the following options:
        Persistent Mode            : Disabled
        Logging Level              : 1
        Listen Port Number         : 61234
        Status Refresh Delay       : 15s
        Verbose Mode               : Disabled
        SWD Debug                  : Enabled
        InitWhile                  : Enabled
 
Failed to bind to port 61234, error code -1: No error
Failure starting GDB server: TCP port 61234 not available.

0 REPLIES 0