cancel
Showing results for 
Search instead for 
Did you mean: 

i need to charge 18650 li ion battery using SPV 1050 MPPT IC. where will i need to connect the load (microcontroller)? on which pin do i need to connect my micro controller?

TVard.1
Associate III

Do i need to connect my load on STORE pin or in parallel to VBATT+ ?

In STEVAL-ISV020V1 what is EXT_SUP? is this where i need to connect my load

what will happen if i discharge 1 Amp current from 18650 battery?

what is the current capacity of inbuilt PASS TRANSISTOR?

0 REPLIES 0