cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IDB05A1 fireware update field!

xqiu.1
Associate

Hi,

I is developing a BLE appilication using X-NUCLEO-IDB05A1 module. I use FlashUpdaterTool (Version 2.1.0) to connent my NUCLEO board of L476RG (VirtualCOMPort Application V0.0.1 ), which connect X-NUCLEO-IDB05A1 module. During updating the fireware, an error was captured, and the application is pended. Therefore, I can not do anything but unplug the USB cable. Then, the FlashUpdaterTool can not find the X-NUCLEO-IDB05A1 module when I unplug again, and the error is as follows,0693W000000WXfzQAG.png

Could anyone tell me what sholu I do to save the life of my NUCLEO-IDB05A1 module?

Kindly regards,

qiuxb@tyust.edu.cn

0 REPLIES 0