2020-03-30 03:42 AM
Hi everyone,
I am interested in buying a P-NUCLEO-IHM03 motor control pack but I would need to find, preferably, encoder or, at least, Hall sensors I can use with the X-NUCLEO-IHM16M1. Could someone please recommend me sensors that work fine with this board ? Thanks in advance.
2020-03-31 06:57 AM
The X-NUCLEO-IHM16M1 have the J1 connector to manage the signal coming from Hall sensors or Encoder.
If you have a BLDC motor integrating the Hall sensors you can use that.
If you are using motor without integrated sensors, we suggest to use a commutation encoders (e.g. CUI devices).
2020-04-03 05:26 AM
Dear CBald.1,
Just one question: with the P-Nucleo-IHM03 there is already a motor provided. Do you plan to use the provided control Nucleo board + IHM16M1 with your own motor?
Thanks,
Claire
2020-04-16 11:17 AM
It also depends on the usecase: If you want to use a bldc for position control (servo... gimbal...), as far, as i know, you HAVE to use incremental encoders (3 lines: A/B/Z (Index)). Refer to https://www.st.com/content/ccc/resource/technical/document/application_note/group1/05/2a/5f/da/fa/91/40/f4/DM00691525/files/DM00691525.pdf/jcr:content/translations/en.DM00691525.pdf in this case.
If you just want to use speed control (6 step or foc), depending on the controller board, it´s not necessary to have any encoder.
With my previous experiences (and disappointed expectations...), when it comes to promoted boards and other stuff, it really helps, if you study the possibilities before you buy anything 😉
2020-10-15 02:48 AM
Dear @CBald.1
Do you have still this problem to solve?
If not, do not hesitate to share the final solution you found.
Best regards
Laurent Ca...
2020-10-26 01:59 AM
Dear @CBald.1
I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting an answer.
Best regards
Laurent Ca...