cancel
Showing results for 
Search instead for 
Did you mean: 

Problem for building my own binary without loosing SD Card detection on the SENSORTILE

MGarb.2
Associate

Hello, 

I'm trying to customize a firmware ALLMEMS2 for the SensorTile evaluation kit.

The binary already built in the firmware folder work well to detect and log data on a SD Card.

But it fail to detect the SD Card when I build my own firmware even if I dont modify the source code.

Do you have some hints to resolve this problem ?

Does STM32CubeIDE need a special configuration to keep this feature ?

1 REPLY 1
RMojt.1
Associate II

Hi,

I think you need to use new SD cards with more than 16GB.

Best,

Ramtin