cancel
Showing results for 
Search instead for 
Did you mean: 

FP AI Sensing enable UART printf issue - sensortile

HKart
Associate II

Halo,

I am using sensortile and currently trying to be familiar with FP AI Sensing. There is an instruction to enable SENSING1_USE_PRINTF in SENSING1_config.h. I did enable it, however there is an error during compilation, and to solve I need to put SENSING1_USE_PWR_MGNT to 0.

The compilation has no error, however my teraterm COM port still doesnt receive any output from sensortile.

Anybody has tried this before?

Thank you

6 REPLIES 6
CPutt.1
Associate III

I am facing same issue...Did you make it work is it something to do with 10s delay?

HKart
Associate II

I didnt manage to make it work. I did confirm that it is not HW issue since I program other FW demo and the UART works.

So it must be the FW issue or I miss out something on the FW steps.

CPutt.1
Associate III

Did you try this initiallization. I will let you if I am able find it out.

CPutt.1
Associate III
 
CPutt.1
Associate III

I also tried it is not working for me as well

NOza.1
Associate II

Hello HKart,

Please find this link for the resolution of this issue.