cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 HAL library release notes are 0.1 off?

Pavel A.
Evangelist III

The latest section in the Release notes html in version 1.7 is numbered 1.8 and has release date 14 Feb. 2020. Version 1.7 there has release date 06 december 2019. Looks like these versions are 0.1 up. The latest release is 1.7 and it should have date around end of Feb. (?)

-- pa

3 REPLIES 3
Amel NASRI
ST Employee

Hi @Pavel A.​ ,

In STM32Cube_FW_H7_V1.7.0/Release_Notes.html, I don't see such misalignment.

0693W000000UdT7QAK.png

Where 1.8 version is mentioned?

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Pavel A.
Evangelist III

Amel,

I apologize, this indeed is not in the released 1.7.0 package. Maybe my version is a preview.

(still in the 1.6 release notes it mentions 1.7)

-- pa

OK, no problem. So it seems already fixed.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.