cancel
Showing results for 
Search instead for 
Did you mean: 

I attach the blender to the reward and the touch button works by itself.

mfurkanuyar
Associate II

Hello to everyone,

I designed a paddle box control card with STM32F042K4T6. The scheme and information of the design are as follows.

Power and Signal

 0690X00000DYppjQAD.jpg0690X00000DYppoQAD.jpg

Button Read Code

0690X00000DYpq8QAD.png

0690X00000DYpqIQAT.png

I don't use Touch Sensing. I only use the TSC unit. I process the value I read later. I didn't add that part to avoid confusion.

I leave it to the test when there is no blender. I encounter this error in 2 out of every 10 cards every 10-12 hours.

If you have a useful idea or criticism, please tell me. I love the STMicroelectronics family.

Thank you.

1 REPLY 1
mfurkanuyar
Associate II

I solved the problem, guys. UT7500 0-3.3V, after 30 milliseconds, but I used the LD of IC firm of ST firm, it reaches 3.3V for 1.2 milliseconds. I also made 470uF and 1000uF right now, there is no problem.