2020-03-04 06:37 AM
Hello,
I'm a student that is currently developing a firmware for a custom board with the STM32WB55CE-MC. I want to communicate with the MC over BT. I have tested my software on the Nucleo-Board where it works fine. When i try the firmware on my custom board, the microcontroller can not be seen in the BLE-Sensor app. While debugging the software, I realized, the MC never leaves the idle-State. I am using STM32CubeIDE for software developement.
Has anybody experienced similar problems?
Do I need to upload firmware to the RF-Core before I can use the BT-Feature? I have not done this up to now but I also have not done this with the Nucleo board.
Thanks in advance for all your answers and kind regards,
Florian P
Solved! Go to Solution.
2020-03-04 06:43 AM
Maybe you have to install the current Firmaware Update Service and the BLE stack, because I think this is not installed when you buy a new MCU.
This was a problem on my custom board with the SMT32WB55CC. After I updated the firmware the BLE stack was started.
Greetings,
Ben
2020-03-04 06:43 AM
Maybe you have to install the current Firmaware Update Service and the BLE stack, because I think this is not installed when you buy a new MCU.
This was a problem on my custom board with the SMT32WB55CC. After I updated the firmware the BLE stack was started.
Greetings,
Ben
2020-03-05 12:37 AM
Hey Ben,
Thanks for your help. I managed to flash the FUS and the BLE stack with CubeProgrammer and now it seems to work. 🙂
Greetings,
Flo