cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STM32H743's FMC drive a 16-bit 8080 bus faster than 1.6MHz when clocked at 480MHz?

CDew.1
Associate III

I'm using the FMC of the STM32H743 to drive a 16-bit 8080-bus LCD controller.

I've tried using DMA, MDMA and a CPU-loop to transfer data to the 8080-bus, via the FMC.

The transfer frequency does not depend on whether DMA, MDMA or CPU-loop is used. This make me think that the DMA/MDMA/CPU-loop is not the limiting factor.

At a 480MHz FMC clock, the transfer happens at just 1.6MHz, giving me only 20fps on a 16-bit colour 320x240 LCD.

At a 240MHz FMC clock, the transfer happens at just 0.8MHz, and so on at slower speeds.

I've also tried reducing the various setup and hold times to 1 and 0 cycles, but this has (surprisingly) not affected the waveform on the 8080-bus.

My (Cube-MX generated) FMC initialisation code is:

 
/* FMC initialization function */
static void MX_FMC_Init(void)
{
 
  /* USER CODE BEGIN FMC_Init 0 */
 
  /* USER CODE END FMC_Init 0 */
 
  FMC_NORSRAM_TimingTypeDef Timing = {0};
  FMC_NORSRAM_TimingTypeDef ExtTiming = {0};
 
  /* USER CODE BEGIN FMC_Init 1 */
 
  /* USER CODE END FMC_Init 1 */
 
  /** Perform the SRAM1 memory initialization sequence
  */
  hsram1.Instance = FMC_NORSRAM_DEVICE;
  hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
  /* hsram1.Init */
  hsram1.Init.NSBank = FMC_NORSRAM_BANK2;
  hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
  hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
  hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
  hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
  hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
  hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
  hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
  hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
  hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_ENABLE;
  hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
  hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
  hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
  hsram1.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
  hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
  /* Timing */
  Timing.AddressSetupTime = 3;
  Timing.AddressHoldTime = 15;
  Timing.DataSetupTime = 4;
  Timing.BusTurnAroundDuration = 1;
  Timing.CLKDivision = 16;
  Timing.DataLatency = 17;
  Timing.AccessMode = FMC_ACCESS_MODE_A;
  /* ExtTiming */
  ExtTiming.AddressSetupTime = 3;
  ExtTiming.AddressHoldTime = 15;
  ExtTiming.DataSetupTime = 4;
  ExtTiming.BusTurnAroundDuration = 1;
  ExtTiming.CLKDivision = 16;
  ExtTiming.DataLatency = 17;
  ExtTiming.AccessMode = FMC_ACCESS_MODE_A;
 
  if (HAL_SRAM_Init(&hsram1, &Timing, &ExtTiming) != HAL_OK)
  {
    Error_Handler( );
  }
 
  HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM);
}

The (Cube-MX generated) clock setup is:

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
  /** Supply configuration update enable 
  */
  HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
  /** Configure the main internal regulator output voltage 
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
 
  while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
  /** Macro to configure the PLL clock source 
  */
  __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLM = 4;
  RCC_OscInitStruct.PLL.PLLN = 480;
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 20;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_1;
  RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
                              |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
  {
    Error_Handler();
  }
  PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SPI1|RCC_PERIPHCLK_USB
                              |RCC_PERIPHCLK_QSPI|RCC_PERIPHCLK_FMC;
  PeriphClkInitStruct.PLL2.PLL2M = 2;
  PeriphClkInitStruct.PLL2.PLL2N = 120;
  PeriphClkInitStruct.PLL2.PLL2P = 8;
  PeriphClkInitStruct.PLL2.PLL2Q = 2;
  PeriphClkInitStruct.PLL2.PLL2R = 1;
  PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_2;
  PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
  PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
  PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_PLL2;
  PeriphClkInitStruct.QspiClockSelection = RCC_QSPICLKSOURCE_D1HCLK;
  PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
  PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL;
  if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Enable USB Voltage detector 
  */
  HAL_PWREx_EnableUSBVoltageDetector();
}

How can I make the FMC on the STM32H743 transfer half-words faster than 1.6MHz, when driven with a 480MHz clock?

(I'd like to achieve 5MHz for 60fps.)

1 ACCEPTED SOLUTION

Accepted Solutions
CDew.1
Associate III

I've changed to using NE1 and continued using 0xC000 0000.

Now that I'm configuring (NE) bank 1 and using NE bank 1, I'm getting 5MHz with just a 48MHz FMC clock and the default timings and clock division.

Previously I was configuring the NE bank 2, but writing to the entirely unconfigured NE bank 1's address. The fact that it worked at all is surprising.

View solution in original post

6 REPLIES 6
Mike_ST
ST Employee

Check the timings...

You can try the following changes

Timing.CLKDivision = 8;

ExtTiming.CLKDivision = 8;

And see whether something happens.

CDew.1
Associate III

@Mike_ST​ I tried that, but it didn't make any difference.

I think I may have spotted the cause of the problem, though I have not yet fixed it.

I have set :

 hsram1.Init.NSBank = FMC_NORSRAM_BANK2;

but I am writing to 0xC000 0000. (When I wrote to 0x6000 0000, before swapping banks, I was getting spurious writes: https://community.st.com/s/question/0D50X00009XkWQE/stm32h743ii-fmc-8080-lcd-spurious-writes .)

I don't care about FMC's chip select, because the LCD is the only other thing on the bus, and its #CS is wired to GND.

I think that the problem is that I'm *configuring* NE bank 2 and then *using* NE bank 1 (by writing to 0xC000 0000).

(The definition of 4 "NE banks" within "FMC bank" 1 confuses me, as it's never clear which type of bank an argument is referring to.)

I will spend some time fixing the hard faults that changing NE2 to NE1 has caused.

Is the address 0xC000 0000 correct to write to NE bank 1 of FMC bank 1 after "HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM);"?

Mike_ST
ST Employee

I don't know how addressing issues can influence timings.

Please check TABLE 147 in RM 0433, maybe that can help a bit.

HAL_SetFMCMemorySwappingConfig(FMC_SWAPBMAP_SDRAM_SRAM); will set BMAP[1:0]=01.

CDew.1
Associate III

I've changed to using NE1 and continued using 0xC000 0000.

Now that I'm configuring (NE) bank 1 and using NE bank 1, I'm getting 5MHz with just a 48MHz FMC clock and the default timings and clock division.

Previously I was configuring the NE bank 2, but writing to the entirely unconfigured NE bank 1's address. The fact that it worked at all is surprising.

CDew.1
Associate III

@Mike_ST​ Thanks for your help. Can you close this ticket please?

You are welcome.

I can't close topics myself, if you like you can flag it as answered, .