cancel
Showing results for 
Search instead for 
Did you mean: 

Steval - spin3204 and motor jk86bls71-03-x001

DTrif.1
Associate

Hello. I am using Steval - spin3204 and motor jk86bls71-03-x001. I am building a project for Keil in ST Motor control 5.4.3. But I can’t start the engine with or without Hall sensors. I tried to make various configurations of PID controllers, PWM parameters, time, etc., but nothing works. Please tell me, if someone has a working project so that I can do it by analogy. A project that is located on the ST website is compiled with errors.

Here is the project I'm working with

1 ACCEPTED SOLUTION

Accepted Solutions
Claire O.
ST Employee

Hello DTrif.1,

Are you using the following example from the MCSDK5.4.3:

  • Six-Step drive with STSPIN3204

Thanks and best regards,

Claire

View solution in original post

1 REPLY 1
Claire O.
ST Employee

Hello DTrif.1,

Are you using the following example from the MCSDK5.4.3:

  • Six-Step drive with STSPIN3204

Thanks and best regards,

Claire