cancel
Showing results for 
Search instead for 
Did you mean: 

I appear to be having some issues with my DFSDM Manchester clock recovery. How do I set up the CKOUT for a 10MHz Manchester input? Do I need any clock connections or does it synchronize itself?

sammerman
Associate

I am using the H7 and have a 10MHz sigma-delta ADC sending the Manchester signal. I do not have a clock going to the ADC because it generates its own.

The internal DFSDM clock is set correctly, I think. I have a system clock of 96MHz and CKOUTDIV is set to 8.

The problem shows itself as readings that jump to the opposite polarity for a dozen or two samples then return to the correct reading.

0 REPLIES 0