2020-02-17 12:21 AM
I'm trying to use Motor Control workbench with BLDC motor (from orbital sander). I ran a test with motor profiler, my motor parameters are the following:
The motor works fine under ~8500 rpm, but above that stops with speed feedback error. With the original control PCB the motor can achieve 11000rpm, but it uses simple b-emf control.
Any recommendation to achieve 11krpm? I tried to use flux weakening feature, but didn't helped.
Thank you in advance!
2020-02-17 12:36 AM
I was wrong, it must be an SM-PMSM motor. The waveform on the windings (if I spin the motor):
2021-06-21 10:59 PM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards