cancel
Showing results for 
Search instead for 
Did you mean: 

Is an example project for STEVAL-CTM010V1 board available?

DKlep.1
Associate
 
2 REPLIES 2
RRach.2
Associate II

Yep, from version 5.4.4+.

But it does not Generate with these versions, it wants 5.4.3 in order to Generate code, where the exmple is missing, but is built for that version.

The error in 5.4.4+ is:

ERROR [LineInfo_to_exitCode.manage_IocGenerationError] Unable to generate ioc file due to: When calling function "name", required parameter "gpio_port" (parameter #1) was specified, but had null/missing value....

Gigi
Senior

Tested right now

Using MC SDK 5.4.8

Opening the example, saving in a folder and generated using the update button

I'm using CubeMX 6.5.0 and Cube IDE 1.7.0

It compile with 0 error 0 warning. Not tested on real board just compilation.

Ciao

Gigi