cancel
Showing results for 
Search instead for 
Did you mean: 

What is the thermal resistance (junction to ambient) for the M24C32?

PLang.2
Associate

No detail about it in the datasheet. This is quite an old part design. I'm looking for the thermal resistance of the industrial version of the part (-40 to 85°C). I'm quite sure that the self-heating is minimum. But, I want characterization data that proves that it is.

1 ACCEPTED SOLUTION

Accepted Solutions
Pierre P.
Senior III

​Hello,

The Value of 'Theta JA' (thermal resistance of junction to air) depends of the package of the EEPROM :

- SO8N (150 mils) : 219°C/W

- TSSOP8: 255°C/W

- MLP 2x3: 67°C/W

- WLCSP : < 40°C/W

BR

Team EEPROM suPPort 

View solution in original post

2 REPLIES 2
Pierre P.
Senior III

​Hello,

The Value of 'Theta JA' (thermal resistance of junction to air) depends of the package of the EEPROM :

- SO8N (150 mils) : 219°C/W

- TSSOP8: 255°C/W

- MLP 2x3: 67°C/W

- WLCSP : < 40°C/W

BR

Team EEPROM suPPort 

PLang.2
Associate

Thanks a lot for the answer.