cancel
Showing results for 
Search instead for 
Did you mean: 

When will we have access to the files for OpenLinux?

KevinA
Senior

In Getting Started there are links to the SDK and Kernel Source, both links return 403 Forbidden They have been broke since Friday evening, at least that is when I tried to install.

7 REPLIES 7
KevinA
Senior

After alerting 'domainabuse@cscglobal.com' about the issue it was finally resolved.

koan
Associate III

The link is working

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package

However, in case you can use the KOAN's unofficial Linux kernel for STM32MP1

https://github.com/koansoftware/linux-stm32mp1-disco

Distinti Saluti / Best Regards

--

Marco Cavallini | KOAN sas | Bergamo - Italia

embedded software engineering

https://KoanSoftware.com

Bernard PUEL
ST Employee

Hello Kevin,

Which links were KO last Friday ? Is it ok now ?

fyi all the ST delivery is also available on Github, see entry point here: https://github.com/STMicroelectronics/STM32MPU_EmbSW_Overall_Offer

I would have to be a lot smarter than I am to use the git. The git has linux 4.19.94 where are the Wiki is 4.19.49 and all the 'parts' are separate git objects instead of a tar file. There was enough differences in the Wiki to make it a struggle to finish, remembering Unix commands that no longer exist sucked, ifconfig is now ip, PS1='\\$' allowed using a 1080 display instead of a 4K with wraparound....

Bernard PUEL
ST Employee

Hello Kevin, we are in the way to deliver V1.2.0. That's why you see a diff between wiki and github. On github you can select the right release tag and extract a zip with the web interface. This zip will contain the linux kernel reference with ST patches.

Bernard PUEL
ST Employee

Anyway, we have investigated the issue about tarball download and if you can login first on st.com you should not have the error 403 anymore.

This issue is on the way to be solved on st.com configuration (normally you can download any openstlinux tarball without any registration).

koan
Associate III

@KevinA​ the KOAN's unofficial Linux kernel for STM32MP1 is exactly what you are looking for.

https://github.com/koansoftware/linux-stm32mp1-disco

It is basically the original Kernel used bt ST with ST patches applied.