cancel
Showing results for 
Search instead for 
Did you mean: 

SPIRIT1 Does not want to generate RF on STEVAL-IKR002V1D

Linas L
Senior II

Hello. I am making RF beacon based on SPIRIT1 RF IC

I downloaded SPIRIT1 DK, configured for 168MHz based on hardware I have, and written CW mode. But with spectrum analyzer with sweep from DC to 1GHz i can't see anything ( same goes if i select 169MHz with 20MHz span)

I confirmed it does write all registers just like in that application, did confirmed that CW bit is set at 0x1B MOD0 bit 7 with modulation scheme OOK as well as maximum power.

Try sending commands after that, like SPIRIT1_TX or SPIRIT1_LOCKTX, did not helped.

What i am doing wrong ? What I am missing ?

0 REPLIES 0