2020-02-01 08:31 AM
Hello,
In stm32h7 I see in the "System architecture" diagram that SRAM3,SRAM2,SRAM1 are not passing through the cache.
Yet, it seems that when using SRAM3 with DMA I must configure it as non-cacheable, otherwise I get junk in data.
Can anyone please explain why it must be configured as non-cacheable in MPU ?
Thanks
2020-02-01 10:12 AM
AN4891 Figure 1. Through what path the CPU accesses the SRAM1-3?
2020-02-01 10:35 AM
2020-02-01 02:22 PM
Looks like the cache is omitted in RM0399 (H7x5/H7x7), but it's properly drawn in RM0433 (H7x3/H750).
Or maybe the I$ and D$ symbols are supposed to mean instruction and data cache? An incredibly lame pun (cash = cache) that has no place in a technical documentation.